Panduit Panduit Panduit UPI

Retirement

Return to the
Benefits page

Panduit offers a 401(k) plan that allows employees to contribute pre-tax salary towards retirement savings. Furthermore, Panduit will partially match employees' contributions to the 401(k) plan as follows:


    Panduit will provide a $1.00 match for each $1.00 an employee contributes to the plan, up to the first 3% of the employee's weekly compensation.
    Panduit will provide a $0.50 match for each additional $1.00 an employee contributes to the plan, up to an additional 2% of the employee's weekly compensation.


In addition, the Panduit Board of Directors determines a profit sharing contribution amount annually based on the company profits. This is calculated as a percentage of an employee's total annual cash compensation and is deposited in a lump sum. The amount of the contribution is declared and the actual contribution is added to the employee’s account in the following year.