globe Australia & New Zealand | English
Product availability varies per region

Part List

Added
item(s) View List >>

Part List

View List >>

Products

Content

Category

Cross References

No Results Found

Capilano University Case Study

At a Glance


Company

Capilano University (CapU)

 

Region / Country

North America/Canada


Industry

Education

 

Panduit Solution

Copper Patch Cords
Fiber Optic Patch Cords
NetKey™ Keystone Patch Panels
2-Post Racks
NetRunner™ Vertical Cable Manager

Connecting to Something New: Copper Connectivity Solutions enable Capilano University to optimize campus operations to improve student and staff experiences.

Panduit optimized the network infrastructure at Capilano University (CapU) to ensure reliable connectivity for +9,000 students and +1,200 employees. Recognizing the critical need for a dependable network, CapU turned to Panduit for its expertise.  Panduit provided advanced copper and fiber network connections in a clean and organized network solution, remarkably reducing downtime and streamlining the troubleshooting process, thereby enhancing the overall education experience.

Challenges

  • Outdated network infrastructure made it difficult to trace and troubleshoot connectivity issues, impacting efficiency.
  • Efficiently troubleshoot outages and keep students and faculty connected
  • Tangled cabling in telco rooms slowed down maintenance, requiring significant time and manpower for troubleshooting


Solution

  • Upgraded the network at Capilano University with Copper Patch Cords, Keystone Patch Panels, and 2-Post Racks
  • Patch cords were color-coded patch cables to identify VLANs, allowing engineers to visually trace connections from patch panel to each switchport efficiently
  • Reduced the ethernet connections needed to fill out the network by 550, making troubleshooting and tracing simpler and eliminating clutter

 

Outcome

  • Significantly reduced time required for troubleshooting, allowing faster resolution for connectivity issues
  • Simplified network maintenance, freeing up IT staff to focus ons trategoic projects
  • Enabled smooth implementation of future network expansions, including planned upgrades to fiber optic systems and the introduction of RapidID Network Mapping system in new campus facilities.

“…Panduit delivered quality manufacturing, R&D, and impressive innovation for even the smallest details… details that some manufactures might overlook…”

– Darin Feist
Network Analyst IT Infrastructure, Capilano University

Challenges

Connectivity is a critical part of modern learning, and never has that been made more apparent than during the global COVID-19 Pandemic. The majority of academia has shifted to online platforms in some capacity. Universities which aim to provide top notch education must use top-of-theline technology to continuously connect students and faculty to each other and more. When technology and resources are unreliable, the academic experiences of students, workplace contentment, and the reputation of the institution can suffer. Outages and errors are unfortunately inevitable in businesses which rely heavily on technology. The best way to quickly and easily trace, troubleshoot, and reestablish stable connections is to build a dependable network infrastructure.

Capilano University is ranked among the top animation and digital design programs in Canada. As is the case in any high-tech environment, reliable equipment is essential.

It was determined that the patch infrastructure and tangled mess of cable in the communications rooms presented several challenges. Maintenance and troubleshooting took longer to complete because of the state of this cabling infrastructure. Effective troubleshooting required a lot more staff and resources, so Panduit stepped in.
 

Another cable management rack with hundreds of cables tangled into a mess, exhibiting network mismanagement prior to Panduit provisions

Figure 1: Previous network setup at Capilano University, illustrating disorganized cabling that made troubleshooting and maintenance challenging and time-consuming

Solution

Maintaining a reliable network infrastructure at CapU keeps the campus running and gives IT Infrastructure time to focus on more rewarding initiatives than troubleshooting outages. Darin Feist shared that the university is focusing on infrastructure  mprovements for operational efficiency gained by the communication room refit.

The scope of this project addressed refitting all 28 telecommunication rooms at Capilano University with a new layout that utilizes Copper Patch Cords, NetKey Keystone Jack Modules, 2-Post Racks, and NetRunner Vertical Cable Managers. The Cedar Building 300 room was a pilot project for CapU to test a new design that was used to upgrade other areas on the campus thereafter.

A new layout improves functionality.

The old layouts for the Cedar 300 Room consisted of 600+ Ethernet connections, where rack layouts previously held switches at the bottom and patch panels at the top. The two were connected by almost 1200 meters of three-and four-meter patch cables.

Elaine Wilson, Panduit Sales Manager for British Columbia, leveraged her expertise to enable university partners to change this room layout using 48 ports of Keystone Patch Panels followed by 48 ports of switch capacity directly below. NetKey is configurable for tight space and the RJ45 interface provides a quick plug-and play connection to patch cords with traceability. This was connected by 200 meters of 28 AWG copper patch cords at standard lengths of 30 cm, which cleaned up the layout by quite a lot.

Cable management rack with populated by patch panel jacks using a color-coding method for the associated VLAN connection documentation

Figure 2: Previous network setup at Capilano University, illustrating disorganized cabling that made troubleshooting and maintenance challenging and time-consuming

Implementation

Darin shared, “Elaine is a great listener and problem solver. She saw our com-rooms and listened to us describe what we needed to make them more ‘serviceable’. She used experiences from other projects to suggest a green-field installation using the short 28 AWG patch cords. Things sort of bloomed from there.”

After the Cedar 300 room was completed, the design was updated with color-coded patch cables in other space to identify VLANs. This allows engineers to visually trace connections from patch panel to switchport. Now, IT staff can walk into a com-room and immediately identify which cables are for a particular VLAN. For example, blue is for students/staff and green means door access.

Creating this bullet-proof method for reliably tracking all VLAN assignments was the most important and challenging component. It condensed the amount of rack-space required for the connections, and the colored patch cords provided a visual map of what was connected to each switch. The team disconnected each patch cable from the switchport, traced them to the patch panel, and swapped them appropriately colored cable according to the color-coding method for the associated VLAN. They populated the patch panel jacks one at a time using, the color-coding method forthe associated VLAN, then reconnected each cord and documented the connection.

The team at Capilano University shared that working with Elaine made this project more enjoyable and manageable. “Her knowledge and attention to detail was most impressive. On top of that, Panduit delivered quality manufacturing, R&D, and impressive innovation for even the smallest details... details that some manufacturers might overlook,” said Darin Feist. This project started in December 2020 and was completed in only nine months. The Panduit team worked tirelessly to procure supplies and labor resources during the height of the COVID-19 Pandemic to take advantage of a student-free campus. Darin says, “The success of this project was based in large part to our relationship with committed industry partners. Elaine deserves many thanks for her commitment and tireless work.”
 

Cable management rack supporting hundreds of short patch cords neatly organized into a rack for easy network mapping as the result of Panduit interventions

Figure 3: Redesigned cable management layout including color-coded patch cables for easy VLAN identification

Outcome

Now, Capilano University IT staff can quickly and easily identify connections from the patch panel to the switch, decreasing the time to troubleshoot, trace, identify, and correct cabling issues.

One month after all existing server rooms were reconfigured, an engineering lab was moved to a different building. The work to configure the communications room to accommodate the changes needed for the lab was completed in only one hour, by one staff member. With the old system, half of a workday may have been spent for such a project.

Upon completion, Capilano University refocused on new projects in which Panduit will bring this new layout, woven with new fiber optic solutions, to the Center for Childhood Studies: a 2,137 square meters, two-story building that will house the School of Education and Childhood Studies. Construction for this space started in Fall 2022. Additionally, the on-site student housing complex will be outfitted with fiber optics. This is a six-story, 8,250-meter complex that can accommodate up to 362 students. Upgrades to this layout will include the RapidID™ Network Mapping System, an autonomous network documentation solution that takes the guess work out of labeling, tracing, and documenting network maps.

Students enjoying various outdoor activities such as studying, frisbee, and spirit activities on the Quad at Capilano University.

Figure 4: Capilano University Campus