Part List

Added
item(s) View List >>

Part List

View List >>

 

Panduit and General Cable to Showcase Campus Connectivity Solutions at BICSI

 

TINLEY PARK, Ill. and HIGHLAND HEIGHTS, Ky. (Feb. 6, 2020) — Panduit, a global leader in innovative electrical and network infrastructure solutions, and General Cable, a global manufacturer of aluminum, copper, and fiber optic wire and cable, will introduce new solutions that enable connectivity between campus buildings during BICSI Winter 2020 Feb. 9-13 in Tampa, Fla. The expanded campus networks offering includes several outdoor-rated enclosures, fiber splice closures, and splicing trays from Panduit, paired with outdoor-rated cables from General Cable, including new hybrid powered fiber cables, which deliver data and power for applications like security cameras and outdoor access points.

The fiber closures are hard molded and hermetically sealed to provide an IP68-rated seal that protects fiber in damp or wet environments. These recently-launched closures pair with fiber splice trays to securely splice fiber either above or below ground. In addition, Panduit has outdoor-rated enclosures for mounting security cameras in outdoor campus spaces.

In the campus space, General Cable offers the industry’s widest breath of copper and fiber cabling options. The offering includes the new GenSPEED indoor/outdoor water impermeable Category 6A plenum rated cable, hybrid fiber/copper cables for extended distances, and a wide range of outside plant constructions, including GenSPEED single mode loose tube outdoor, aerial lashed, duct, and direct buried cables, as well as indoor/outdoor configurations and ribbon fiber for mass fusion termination.

The complete campus network solution can be seen in the Panduit and General Cable booth (#701) at BICSI Winter 2020. In addition, visitors can see how the PanGen offering helps connect digital buildings, along with industrial and data center applications, Panduit and Atlona’s end-to-end AV solution, and General Cable’s extensive cabling portfolio, including new packaging options.   

About General Cable: General Cable – one of three distinct commercial brands (Prysmian, Draka and General Cable) of the Prysmian Group – with headquarters in Highland Heights, Kentucky, is a global leader in the development, design, manufacture, marketing and distribution of aluminum, copper and fiber optic wire and cable products for the energy, communications, transportation, industrial, construction and specialty segments.

From a cable producer supplying to several industries, to a technology enabler making progress happen, General Cable provides customers and communities worldwide with cable solutions based on state-of-the-art technology, consistent excellence in execution and in-depth understanding of the needs of an evolving market.

About PanGen: Since 2004, Panduit and General Cable’s world-class partnership has provided infrastructure solutions, guaranteed network performance and system reliability. All PanGen installations are eligible for a complete 25-year solution warranty, offered through an extensive network of specially certified installers.    

About Panduit

Since 1955, Panduit’s culture of curiosity and passion for problem solving have enabled more meaningful connections between companies’ business goals and their marketplace success. Panduit creates leading-edge physical, electrical, network infrastructure and AV solutions for enterprise-wide environments, from the data center to the telecom room, from the desktop to the plant floor. Headquartered in Tinley Park, Ill., USA and operating in 112 global locations, Panduit’s proven reputation for quality and technology leadership, coupled with a robust partner ecosystem, help support, sustain, and empower business growth in a connected world.

 

 

Press Contact