Part List

Added
item(s) View List >>

Part List

View List >>

Securing Connectivity: The Vital Role of Grounding in Protecting and Enhancing Broadband Systems

Sep 2023
Electrical Infrastructure Broadband
A technician on a ladder enhancing fiber optics cables

A broadband system is a network that uses a wide range of frequencies to transmit data. This allows for more data to be transmitted at the same time, which results in faster speeds. Broadband systems are used to deliver high-speed internet connections, and they can also be used to transmit other types of data, such as voice and video.

There are several different types of broadband systems, including:

Cable Modem broadband: Cable broadband systems use the same cables that are used to deliver cable television. They are one of the most common types of broadband systems, and they offer speeds of up to 1 gigabit per second (Gbps).

DSL broadband: DSL broadband systems use the same phone lines that are used for traditional landline telephone service. They are a good option for people who do not have access to cable broadband, and they offer speeds of up to 100 Mbps.

Fiber optic broadband: Fiber optic broadband systems are the fastest type of broadband system. They use fiber optic cables, which are made of glass or plastic. Fiber optic broadband systems can offer speeds of up to 10 Gbps.

Satellite broadband: Satellite broadband systems use satellites in space to transmit data. They are a good option for people who live in rural areas where other types of broadband systems are not available, and they offer speeds of up to 100 Mbps.

Wireless Broadband: Wireless systems connect homes and businesses to the Internet using a radio link between the customer’s location and the service provider’s facility. Wireless Broadband offers speeds of up to 5Gbps.

Which Broadband systems require grounding?

Broadband grounding is the practice of connecting the metallic components of a broadband system to earth ground. This helps to protect the system from lightning strikes and other electrical disturbances such as noise currents which can inhibit the functionality of the system. It also helps to reduce the risk of shock or fire.

The National Electrical Code (NEC) requires that all broadband systems that use metallic components be grounded. This includes cable broadband systems, DSL broadband systems, and fiber optic broadband systems. The grounding helps to protect the system from lightning strikes and other electrical disturbances such as current surges.

The grounding requirements for broadband systems are specified in Article 800 of the NEC. The grounding conductor must be a copper wire that is at least 14 AWG in size. The grounding conductor must be connected to the metallic components of the system, such as the cable, the modem, and the grounding block. The grounding conductor must also be connected to the earth ground, via metal water supply pipe or a ground rod.

If you are installing a new broadband system, or if you are upgrading an existing system, be sure to have it properly grounded.

There are two main types of broadband grounding:

  • Bonding:  This includes components like coaxial cables, network interface units (NIUs), and grounding blocks. The purpose of this bonding is to create a direct link between these components, ensuring they share the same electrical potential. By doing so, Panduit's bonding approach helps to prevent potential differences between these components, which could lead to issues like arcing or other electrical problems.
  • Grounding: Panduit provides solutions that involve connecting bonded components to an earth ground. This can be achieved through methods like attaching the components to a metal rod driven into the ground or connecting them to a metal water pipe that is buried underground. By establishing this connection to the earth, any excess electrical charge or potential can be effectively discharged, ensuring the safety and proper functioning of the electrical and network infrastructure.
     

Grounding is an important part of any broadband system. It helps to protect the system from damage and to reduce the risk of shock or fire. If you are installing a new broadband system, or if you are upgrading an existing system, be sure to have it properly grounded.

Grounding broadband systems is an important safety measure that can help to protect your system from damage and to improve signal quality. Here are some of the benefits of grounding broadband systems:

  • Protects the system from lightning strikes: Lightning strikes can cause serious damage to broadband systems. Grounding helps to dissipate the electrical current from a lightning strike, which can help to protect the system from damage.
  • Reduces the risk of shock or fire: Grounding helps to equalize the potential between the different components of the system, which can help to prevent arcing or other electrical problems. This can reduce the risk of shock or fire.
  • Improves signal quality: Grounding can help to improve the signal quality of a broadband system. This is because grounding helps to reduce noise and interference, which can improve the clarity of the signal.
     

Here are some specific examples of how grounding is used inside plant (central office):

  • The frames of all equipment racks and cabinets are grounded. This helps to protect people from electrical shock and to prevent noise and interference in telecommunications signals.
  • The shields of all cables are grounded. This helps to protect the signals from noise and interference.
  • The power supply for all equipment is grounded. This helps to protect the equipment from damage and to improve the performance of the signals.
  • The building itself is grounded. This helps to protect people from electrical shock and to prevent lightning strikes from damaging the equipment.
  • Here are some specific examples of how grounding is used outside plant (OSP):
  • The metal messenger strand that supports aerial cables is grounded. This helps to protect people from electrical shock and to prevent lightning strikes from damaging the cables.
  • The shields of all buried cables are grounded. This helps to protect the signals from noise and interference.
  • The power supply for all OSP equipment is grounded. This helps to protect the equipment from damage and to improve the performance of the signals.
  • All metal poles and other structures that support OSP equipment are grounded. This helps to protect people from electrical shock and to prevent lightning strikes from damaging the equipment.
     

The grounding system within an inside plant (central office) or outside plant (OSP) network is typically a complex system that includes multiple grounding rods, cables, and other components. The system is designed to provide a low-impedance path to the ground for all currents that flow through the equipment.

Here are the steps on how to properly ground a broadband system:

  • Identify the grounding point. The grounding point is the point where the grounding conductor will be connected to the earth. This could be a metal water pipe, a metal rod that is driven into the ground, or a grounding electrode that is installed by a qualified electrician.
  • Connect the grounding conductor. The grounding conductor is the wire that will connect the grounding point to the metallic components of the broadband system. The grounding conductor must be a copper wire that is at least 14 AWG in size.
  • Bond the metallic components. The metallic components of the broadband system must be bonded together. This means that they must be connected to each other with a copper wire that is at least 14 AWG in size.
  • Test the grounding system. Once the grounding system is installed, it must be tested to make sure that it is working properly. This can be done by using a megohmmeter to measure the resistance of the grounding system.
     

Grounding a broadband system is an important safety measure that can help to protect the system from damage and to improve signal quality. If you are considering grounding your broadband system, be sure to have it installed by a qualified electrician.

If you are considering grounding your broadband system, there are a few things you need to keep in mind:

  • The type of grounding system you need will depend on the type of broadband system you have. For example, a cable modem will require a different grounding system than a DSL modem.
  • The grounding system must be installed by a qualified electrician. Improper grounding can be dangerous, so it is important to have the system installed by a professional.
  • The grounding system must be inspected regularly. The grounding system should be inspected periodically to make sure that it is still in good condition.
     

Grounding your broadband system is an important safety measure that can help to protect your system from damage and to improve signal quality.

For more information about the benefits of partnering with Panduit for broadband projects, check out this short video.

Author:

Ray Froude

Ray Froude is the Sr. Product Manager of power connectors, grounding, and associated tools for Panduit’s Industrial Electrical Infrastructure business.