Part List

Added
item(s) View List >>

Part List

View List >>
Awards & Achievements

Industry recognition for our innovation and customer collaboration

 A diverse crowd of people enthusiastically clapping together, showcasing unity and celebration in a lively atmosphere.
  • Panduit VeriSafe™ 2.0 Absence of Voltage Tester and Occupational Health and Safety Industrial Hygiene Award logo

    2023 Occupational Health & Safety Industrial Hygiene Award-Facility Safety

    VeriSafe™ 2.0 Absence of Voltage Testers

    OH&S recognized the VeriSafe 2.0 Absence of Voltage Tester for its innovative way to test for the absence of voltage safely, reliably, and efficiently with exposure to electrical hazards.

    Product Details
    Read the Press Release

    Gallagher Best in Class Employer

    2022 Best in Class Employer

    Panduit Recognized by Gallagher

    Panduit was one of the 4,000 participating organizations in the 2022 Benefits Strategy & Benchmarking Survey, which forms part of Gallagher’s influential U.S. Workforce Trends Report Series.

    Join Our Team

    Multi-level school along the waterfront

    2022 Cabling Innovators Award-Platinum Level

    GIGA School Concept Application

    The winning case study application highlighted how Japan’s Kawachinagano City Board of Education selected Panduit products for all the wiring materials and parts to be installed for their GIGA schools including its Advanced Vari-MaTriX Category 6A cables, field term plugs, and patch cords.

    Read the Case Study
    Read the Press Release

    RapidID scanner, iPad screen with RapidID logo, and barcode on patch cord cable.

    2022 Cabling Innovators Award-Platinum Level

    RapidID™ Network Mapping System

    CI&M recognized the innovative RapidIDNetwork Mapping System as a practical alternative to traditional manual approaches to the cable documentation process with a solution using patch cords pre-labeled with unique barcodes and a Bluetooth®-enabled handheld scanner to automate labeling, tracing, and troubleshooting.

    Product Details
    Read the Press Release

    Image of four different Panduit FieldCord connectors

    2022 Cabling Innovators Award-Gold Level

    FieldCord™ Connector

    The FieldCord™ Connector was recognized by CI&M for being designed specifically to connect devices such as cameras and access points that have small openings for cords or plugs.

    Product Details
    Read the Press Release

    FlexCore™ Optical Distribution Frame product with cabinet doors open showing yellow cables

    2022 Cabling Innovators Award-Gold Level

    FlexCore™ Optical Distribution Frame

    The FlexCore™ ODF system was recognized for enabling a consolidated patch cord length to be used between a single, double, or quad frame arrangement, freeing up capital that is tied up in holding inventory, and ensuring the customer always has the right parts on hand.

    Product Details
    Read the Press Release

    Two PanMPO Connectors (green/yellow and blue/black)

    2022 Cabling Innovators Award-Gold Level

    PanMPO™ Fiber Connector

    The enhanced PanMPO™ Fiber Connector was recognized by CI&M for its innovative push-pull boot that allows for easy installation and removal, as well as it has the ability to change gender and polarity without additional tools. 

    Watch the Video
    Read the Press Release

    Two SmartZone UPS products stacked

    2022 Cabling Innovators Award-Gold Level

    SmartZone™ Uninterruptible Power Supply

    The SmartZone™ UPS was recognized by CI&M for its delivery of highly efficient and reliable power protection and backup power for IT equipment by providing excellent electrical performance, intelligent battery management, enhanced intelligent monitoring, secure network functions, and a long lifespan for lithium units.

    Product Details
    Read the Press Release

    Wire Basket Overhead Cable Tray Routing System

    2022 Cabling Innovators Award-Silver Level

    Wire Basket Overhead Cable Tray Routing System

    The Wire Basket Overhead Cable Tray Routing System was recognized for contributing to effective space utilization, reduced installation time, and network performance by providing a greater strength-to-weight ratio than other wire baskets as well as the design of its wire mesh grid pattern which allows greater amounts of cables and QuickNet Cassettes to pass grid openings without additional cutting.

    Product Details
    Read the Press Release

  • Single Pair Ethernet Cable

    2021 Cabling Innovators Award-Platinum Level

    Single Pair Ethernet

    Single Pair Ethernet, receiving platinum honoree, is a seamless single protocol network from application edge to the cloud. SPE simplifies network design and operation, eliminating the support and translation of legacy network protocols used in OT networks.

    Learn More

    PanZone® TrueEdge™ Wall Mount Enclosure

    2021 Cabling Innovators Award-Gold Level

    PanZone® TrueEdge™ Wall Mount Enclosure

    The PanZone® TrueEdge™ Wall Mount Enclosure, receiving gold honoree, minimizes network infrastructure investment by providing a solution to eliminate a rack or cabinet.

    Watch Video
    View Solution

    FlexFusion Cabinet

    2021 Cabling Innovators Award-Gold Level

    FlexFusion™ Cabinet

    The FlexFusion™ Cabinet, receiving gold honoree, offers a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge, and Colocation. The cabinet is built with a best-in-class weight load of 3,500 lbs., doors with a maximum airflow of 80%, and custom configurations to meet network needs.

    Learn More
    View Solution

    Adjustable Depth 4-Post Racks

    2021 Cabling Innovators Award-Silver Level

    Adjustable Depth 4-Post Racks

    Adjustable Depth 4-Post Racks, receiving silver honoree, combine the stability of a cabinet with the accessibility of an open rack to provide users with maximum flexibility when designing the network layout.

    View Selection Guide
    View Solution

    TX6A™ FieldCord™ Connectors

    2021 Cabling Innovators Award-Silver Level

    TX6A™ FieldCord™ Connectors

    The TX6A™ FieldCord™ Connectors, receiving silver honoree, enable connection to devices in the most confined cable routing paths and has the capability to be re-terminated up to 20 times with no additional parts.

    Watch Video
    View Solution

    Image of the HD Fusion Wall Mount Enclosure

    2020 Cabling Innovators Award-Gold Level

    HD Fusion Wall Mount Enclosure

    The HD Fusion Wall Mount Enclosure was recognized by CI&M as a fiber cabling solution that houses, organizes, manages, and protects cable-to-cable fusion splice connections and comes in two different sizes to splice up to 3,456 fibers or 6,912 fibers. 

    Product Details
    Read the Press Release

    Image of HD Flex™ Zone Raised Floor Enclosure

    2020 Cabling Innovators Award: Gold Level                                                       

    HD Flex™ Zone Raised Floor Enclosure

    CI&M recognized the HD Flex™ Zone Raised Floor Enclosure as a structured cabling solution that saves valuable real estate in the data center by allowing cable terminations below raised floors, helping to relieve rack and cabinet congestion. 

    Product Details
    Read the Press Release

    UC Davis Medical Center Building with Palm Trees and Signage

    2020 Cabling Innovators Award: Platinum Level

    UC Davis Medical Center

    The CI&M Platinum winning case study highlights the 14-year partnership between UC Davis Medical Center, Panduit, and General Cable. The medical center is supported by four data centers (one on-premises and three colocation facilities), and more than 250 telecommunications rooms. The campus has more than 70,000 cable drops, equating to more than 140,000 Panduit connectors, and more than 12 million feet (more than 2,300 miles) of cable.

    Read the Case Study
    Read the Press Release

    Image of white PatchRunner 2 Cable Management System

    2020 Cabling Innovators Award: Gold Level

    PatchRunner™ 2 Cable Management System

    CI&M recognized the PatchRunner™ 2 Cable Management System as a cabling solution that manages growing cable densities, larger network equipment, and increasing energy usage.

    Product Details
    Read the Press Release