Ultra-Resistant New Nylon Cable Ties Expand Outdoor Capabilities
Nylon 612 UV-resistant
UV-Resistant nylon 612 offers a 20-year guaranteed service life
Panduit Nylon 612 high strength cable ties are resistant to chemical corrosion, solar radiation, and acid rain
Designed for harsh external applications, and guaranteed operating temperature range -60oC to 90oC
FRANKFURT AM MAIN, 11.11.2022 – Panduit has launched a range of harsh environment and UV-resistant cable ties, the PLT4S-M6120, manufactured in resilient nylon 612 with a guaranteed 20-year life cycle. Panduit’s PLT4S-M6120 cable ties are resistant to chemical corrosion, even salts, hydrocarbons, chlorinated hydrocarbons, bases, or corrosive substances such as zinc chloride or diluted acids, making them ideal for harsh outdoor applications. The robust material properties of nylon 612 also ensure continuous stable hold in position for cable or pipe work across the ambient temperature range of -60oC to 90oC guaranteeing a wide application including high wind and high vibration surfaces.
Limited availability of nylon 12 on the world market and the 15% cost advantage of nylon 612 over nylon 12 makes Panduit’s new cable tie attractive for numerous applications in industry and renewable energy systems.
The Panduit fasteners are ideal for cable management on galvanized surfaces and frames, for example, in the growing market for photovoltaic systems. Available in black nylon, the cable ties have a one-piece design with a locking wedge and a curved, tapered tip requiring less insertion force. The PLT4S-M6120 is easy to install increasing reliability and raising overall productivity.
About Panduit
For more than 60 years, Panduit has been the world’s leading provider of innovative solutions in the field of physical and electrical infrastructure for data centres, industrial and building automation and related services. Headquartered in Tinley Park, Illinois, USA with offices in 112 locations worldwide, Panduit stands for quality and innovative technologies. The family-owned company with more than 5,500 qualified employees generates sales in the billion Euro range worldwide. Panduit owes its outstanding market position to the constant striving for innovation and the untiring commitment of its employees. The global player invests above average in research and development, in first class production, in the best possible support of its sales channels and in excellent customer service. This, combined with a strong partner network, is the prerequisite for comprehensive support, sustainability and solid corporate growth in the networked world of today and tomorrow.