No Results Found

PRESS RELEASE

Safely germ-free with antimicrobial cable ties

Antimicrobial and metal-detectable cable ties and mounts for hygiene-sensitive areas

FRANKFURT AM MAIN, 28.02.2024 – With its antimicrobial and metal-detectable cable ties and fasteners, Panduit is expanding the range of applications for medical technology, food production, laboratories and the pharmaceutical industry, among others. The fastening components are made from a metal-impregnated material and can be identified by metal detection devices. The cable ties comply with Hazard Analysis and Critical Control Points (HACCP) specifications, the North American standard of the U.S. Food and Drug Administration (FDA), and the hygiene regulations of the European Union (EU). In addition, the components are provided with an (Environmental Protection Agency) EPA-registered, antimicrobial and ionised additive that prevents the growth of various bacteria, moulds and fungi on the product surface in independent laboratory tests in accordance with ISO 22196:2019 and ASTM G21-15. This reduces the formation of harmful germs and odours, improves hygiene and increases safety in critical areas of application. The cable ties ensure a reliable hold in the operating temperature range between -60°C and 85°C in accordance with UL746B and are resistant to chemicals.

The innovative cable ties from Panduit offer triple protection: thanks to their antimicrobial properties, they prevent contamination. The material mix of nylon 6.6 and the integrated mini metal parts facilitate machine identification and the bright blue colour allows the components to be quickly identified by eye. This means that the cable ties can be quickly detected and, if necessary, removed during the various production phases. Panduit's antimicrobial cable ties are an innovative solution for fastening cables and wires effectively, simply and securely. At the same time, they inhibit the growth of microorganisms and improve hygiene in environments with a high germ load for greater safety.

Antimicrobial and metal-detectable cable ties and mounts
About Panduit


For more than 60 years, Panduit has been the world’s leading provider of innovative solutions in the field of physical and electrical infrastructure for data centres, industrial and building automation and related services. Headquartered in Tinley Park, Illinois, USA with offices in 112 locations worldwide, Panduit stands for quality and innovative technologies. The family-owned company with more than 5,500 qualified employees generates sales in the billion Euro range worldwide. Panduit owes its outstanding market position to the constant striving for innovation and the untiring commitment of its employees. The global player invests above average in research and development, in first class production, in the best possible support of its sales channels and in excellent customer service. This, combined with a strong partner network, is the prerequisite for comprehensive support, sustainability and solid corporate growth in the networked world of today and tomorrow.

Press Contact


Patrick-Steeven Skwara
Marketing Manager
Patrick.Skwara@panduit.com
Tel. +49 6196 78530 27

Martin Kandziora
Senior Marketing Manager EMEA 
Martin.Kandziora@panduit.com 
Tel. +49 6196 78530 46